Danfoss Logo
Home Sitemap Worldwide
InfoEmail
HVACity
Drives Overview
Glossary
Technical Notes
Features
Fast Path
www.danfoss.com/drives

Cooling Tower Fans - Application Description

Traditional solution | New standard | Energy Savings
Click here to read more about: AEO, PID Control, VVC plus, Sleep Mode

Application Description
Cooling towers are used to cool condenser water in water-cooled chiller systems, the most efficient means of creating chilled water. The tower fans provide moving air to cool the condenser water by evaporation. After passing through the tower, the cooled water collects at the bottom of the cooling tower basin and is pumped back through the chiller condenser by the condenser water pump. In many climates, cooling towers provide the most energy efficient method of removing heat from the chillerís condenser water. More...

      Next