Danfoss Logo
Home Sitemap Worldwide
InfoEmail
HVACity
Drives Overview
Glossary
Technical Notes
Features
Fast Path
www.danfoss.com/drives

Car park - Energy Savings Over Time

Application Description | Traditional Solution New Standard
Click here to read more about: AEO, PID Control, VVC plus

Energy savings over time
To calculate the potential savings over time, the actual load/time profile must be known. The load profile indicates the amount of flow the system requires to satisfy its loads during a typical day, month, year or time period under study. The diagram below (Energy consumption over time) shows a typical load profile of a HVAC system. This profile will vary depending on the specific needs of the system due to geographical location, requirements from authorities, safety margins used in the design phase and several other factors.

      
                                                                                                                                                              Previous