Danfoss Logo
Home Sitemap Worldwide
InfoEmail
HVACity
Drives Overview
Glossary
Technical Notes
Features
Fast Path
www.danfoss.com/drives

Condenser Water Pumps - Application Description

Traditional solution | New standard | Energy Savings
Click here to read more about:  AEO, PID Control, VVC plus

Application Description
Condenser water pumps are used to circulate water through the condenser section of a water-cooled chiller and the associated cooling tower.  The condenser water absorbs heat from the chillerís condenser section and releases it into the atmosphere in the cooling tower by evaporation.  These systems are used to provide the most efficient means of creating chilled water, being as much as 20% more efficient than smaller air cooled chillers.



  Next