Danfoss Logo
Home Sitemap Worldwide
InfoEmail
HVACity
Drives Overview
Glossary
Technical Notes
Features
Fast Path
www.danfoss.com/drives

Condenser Water Pumps - New Standard

Application Description | Traditional Solution | Energy Savings
Click here to read more about:  AEO, PID Control, VVC plus

New Standard
Adjustable frequency drives can control condenser water pumps without the need to balance the system with a throttling valve.  Using a drive rather than a throttling valve saves the energy that would have been absorbed by the valve.  Reduced pressure operation can be accomplished with manual speed control of the drive to reduce the pump capacity, resulting in a constant speed, constant volume application of the drive.  This can amount to savings of 15-20% or more. More...


Click on graphic to animate!

 Previous   Next