capacitance
The
measure of the electrical effect of a capacitor. This is often expressed in
microfarads (mF) or picofarads (pF).
capacitor
A
device that is used in electrical circuits to store an electrical charge on sets
of internal plates. Its value is often measured in microfarads (mF) or
picofarads (pF), and is also rated by the maximum voltage that can be applied to
it. Capacitors are often used to correct the phase-shift power factor which AC
induction motors cause. A capacitor used in conjunction with a coil can produce
a resonant or "tuned" circuit.
carrier
frequency
In
a PWM inverter, this is the fixed rate at which voltage pulses are provided to
the motor. Carrier frequencies from 1 kHz through 20 kHz are common.
CENELEC
ComitÈ
EuropÈen de Normalisation Electrotechnique. CENELEC
is the European Committee for Electrotechnical Standardization. Founded 1973 as
a non-profit-making organisation under Belgian Law. It has been officially
recognised as the European Standards Organisation in its field by the European
Commission. Its members have been working together in the interests
European
harmonisation since the late fifties, developing alongside the European Economic
Community.
chassis
ground
A
ground connection made to the metal chassis on which the components of a circuit
are mounted.
choke
A
coil used in a direct current circuit to smooth out a pulsating wave form to
reduce ripple.
chopper
An
internal circuit in some adjustable frequency drives which regulates output
voltage by quickly turning on and off the power applied to the output section of
the drive. Drives which use a chopper to control output voltage commonly use a
diode bridge rectifier input section.
clock
frequency
The
frequency, measured in Hz, of an oscillator used to time or synchronize the
operations of a computer or a microprocessor. The higher the clock frequency,
the faster the operation of the computerized circuit. Several international
boards regulates the radio-frequency emissions caused by oscillators with a
frequency of 10 kHz or higher.
closed
loop
A
regulator circuit in which the actual value of the controlled variable (such as
pressure, temperature or speed) is sensed and a signal proportional to this
value (feedback signal) is compared with a signal proportional to the desired
value (set point signal). The difference between these signals (error signal)
causes the controlling device to change in the direction that will reduce the
difference in signals to zero.
cogging
A
condition in which the motor does not rotate smoothly, but steps from position
to position while rotating. This may occur at very low speeds when the motor is
driven by an adjustable frequency drive.
common
mode voltage
Voltage
between a wire and circuit common or earth ground.
commutation
In
an SCR circuit, momentarily reversing the polarity to turn the SCR off.
conducted
noise
Electrical
noise that travels along the power wiring of a building. Also called EMI.
When operated above base speed with an adjustable frequency drive, the speed
range where base speed horsepower/kW can be utilized.
constant
torque load
A
mechanical device which requires approximately the same torque at all operating
speeds. Starting torque requirements may be significantly greater than running
torque.
constant
torque range
When
operated below base speed on an adjustable frequency drive, the speed range
where base speed torque can be utilized.
constant
volts per Hertz
(V/Hz)
A description of one way an adjustable frequency drive varies the output voltage
to be directly proportional to the frequency at all times. This is necessary for
the motor to produce full torque over the operating speed range.
contactor
A
two-state (on or off) device for making and breaking an electric power circuit.
contactor
bypass
A
three position (drive, off, line) selector switch that electrically selects
whether the motor is driven by the drive, the line or disconnected from both.
Both the motor starter, supplied inside the drive enclosure, and the contactor
for the drive are controlled by this selector switch. A light usually indicates
if the motor is running from the line. Terminals are available to remotely
control the bypass, and to remotely indicate drive or line operation. (see
automatic bypass and fused power disconnect)
contactor
motor selection
This
selector switch electrically transfers the drive from one motor to another by
opening and closing contactors mounted in the drive enclosure. This allows the
drive to operate either one motor or the other at adjustable speed. A terminal
strip is available, if specified, for remote actuation of the contactors.
contactor
reversing
An
electro-mechanical method of reversing motor rotation by using two contactors.
One contactor produces rotation in one direction, the other produces rotation in
the other direction. They are interlocked so that both cannot be energized at
the same time.
continuous
rating
The
maximum constant load that can be carried indefinitely without exceeding
temperature and/or other established limitations of the motor, adjustable
frequency drive, or driven equipment.
control
circuit
The
circuit which carries the electric signals directing the performance of a
controller, but not carrying the main circuit power.
converter
(Electronic)
A device to change DC to AC. e.g., a rotary converter or a solid state
converter. An adjustable frequency drive is in part a solid state converter.
cos(–)
Displacement
(or phase shift) power factor. The angle – indicates the number of degrees of
displacement that exists between the voltage and current waves. Technically,
displacement power factor describes only one aspect of total power factor, but
most commonly, the term "power factor" is assumed to mean
"displacement power factor".
counter
EMF
Counter
electromotive force. Voltage induced in an inductor or the armature coil of a
motor by the flow of changing current through the inductor or armature. The
polarity of this voltage is opposite (counter) to that of the change of current.
Also called back voltage.
critical
speed step-over
A
circuit in an adjustable speed drive that can be adjusted to assure that the
resonant speed or speeds of a cooling tower, vane axial fan or other driven
system can be avoided.
C-UL
Canadian Underwriters Laboratories
A
product safety certification and listing service available through Underwriters
Laboratories, Inc. that is accepted by federal, provincial and local authorities
in Canada.
current
Measure
of the rate of flow of electrical charge. This is measured in amperes (A), or
amps.
current
limit
Electronic
drives have circuitry that automatically controls the maximum output current of
the drive. This is necessary to protect the current carrying components.
Typically the drive’s rating is at 100% current. Constant torque drives
typically have a maximum current limit of 150%, variable torque drives a maximum
current limit of 100 to 115%.
current
source drive
An
adjustable frequency drive that directly controls the current supplied to the
driven motor. Such drives use a large inductor to help control current. While
current source drives had been common in the past, they are now mostly reserved
for drives larger than 300 HP/225kW and for applications where fast load
reversals will be present.