Danfoss Logo
Home Sitemap Worldwide
InfoEmail
HVACity
Drives Overview
Glossary
Technical Notes
Features
Fast Path
www.danfoss.com/drives

Pressure Booster Pumps - New Standard

Application Description | Traditional Solution | Energy Savings
Click here to read more about: AEO, PID Control, VVC plus, Sleep Mode

VLT frequency converters can be added to pressure booster pumps as an alternative to using pressure control valves. This saves the energy that would have been absorbed by the valve and eliminates its cost and maintenance. The savings often amount  to 20% or more,  simply due to the safety factor      used during the design of the system. If the suction pressure of the pump varies, the over-sizing of the pump required to handle the lowest suction pressure does not penalize the installation, when the suction pressure increases. More...

 


Previous      Next