Danfoss Logo
Home Sitemap Worldwide
InfoEmail
HVACity
Drives Overview
Glossary
Technical Notes
Features
Fast Path
www.danfoss.com/drives

Secondary Pumping - Energy Savings

Application Description | Traditional solution | New Standard
Click here to read more about: AEO, PID Control, VVC plus, Sleep Mode

Energy Savings
The way an adjustable frequency drive and variable speed pump respond to the system curve is shown in the diagram. The control curve shows the actual operation points of the secondary pump with variable speed control. The setpoint is the amount of pressure that must be maintained, at the sensor location, even at zero flow, to satisfy system requirements such as minimum pressure differential to operate the coils and control valves. The lower the setpoint, the greater the potential savings, as shown in the diagram. More...


Click on graphic to animate!

Previous    Next