Danfoss Logo
Home Sitemap Worldwide
InfoEmail
HVACity
Drives Overview
Glossary
Technical Notes
Features
Fast Path
www.danfoss.com/drives

Smoke Extract - Application Description 

Traditional solution | New standard  
Click here to read more about:  VVC plus

Application Description
Smoke extract systems are used in large buildings to remove smoke from the building in the event of fire.

They also prevent smoke from circulating from contaminated or smoke-filled zones to uncontaminated zones

The system interacts with the building’s ventilation system and is triggered by a dedicated controller that is integrated with the fire alarm system.

 

 

 

 

 

 

 

 


     Next